Hi Dean / Ti team,
I am using the TICSPRO with the LMX2492EVM
I have replaced the macom VCO MAOC-009265 (outputting 9.4-10.8GHz) with pin-compatible MAOC-009260 (outputting 6.1-7GHz for the same Vtune)
I need to output the following REPEATING chirp via the LMX2492EV, via its RF/2 port:
Fstart = 3.05GHz
Fstop = 3.5GHz
Chirp duration 6500uS
# of steps within the chirp = 65,536 (2^16)
can you please assist me with how to do this via the TICSPRO or best send me a reference *.TCS file.
I would highly appreciate it.
Much thanks for your time.
Ehud