Other Parts Discussed in Thread: LMK04808
I have a customer designing with LMK04828.
They are using the Crystek CVHD (at a different frequency). Here are their questions:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a customer designing with LMK04828.
They are using the Crystek CVHD (at a different frequency). Here are their questions:
The LMK04828 supports placing a crystal on OSCin. However if you're using a CVHD VCXO, you are using a part with an output buffer so there is no need to worry about the crystal specifications. The schematic as given above can be used except you may pick different C4 or C33 values (or just remove C33). C33 can help with filtering some higher order harmonics of the VCXO.
> So in this case, the 10 to 40 MHz is not applicable, the up to 500 MHz is what you'll be working with.
If you do want to use the crystal feature, the LMK04808 datasheet has some more application info/example in section 9.1.8 on page 109 you may look into.
Gregory Duperon said:The CVHD has a load capacitance of 14pF, whilst I believe the LMK presents a 1pF input. I might be misreading the datasheet as the section is as follows:
Let me know if this answer misses the mark or helps clarifies your question.
73,
Timothy