Part Number: TPL5110-Q1
Hi Team,
I am considering to use a TPL5110-Q1 for power saving, by enabling the main 5 V supply through a pMOS around every second (tIP–50 ms).
I would connect the DONE pin to ground, and the DRV pin to a nMOS that switches the pMOS ON for around 50 ms and OFF for tIP-50 ms (1 sec).
If possible, I have some questions about the component:
1) May I connect the DONE pin directly to ground?
2) How much is the max current the push-pull DRV pin can manage safely?
3) When the DONE pulse is not served the DRV pin goes high after tIP for typ. 50 ms; after this time, dose it turn low again for tIP-50 ms ? looking at fig.8 of the datasheet it could seem it stays high for another time.
4) May you tell the min and max value of this "50 ms" time? for instance, if it could be as low as 20 ms or as high as 200 ms I have to think to another implementation. On the contrary, if you could confirm it varies within 40-60 ms it would be great.
Thank you in advance for what you can answer
Kind regards,
Alberto Carlotti