This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2820: Confirmation regarding SYSREF divider

Part Number: LMX2820
Other Parts Discussed in Thread: PLLATINUMSIM-SW

Hi Team,

Our customer's original inquiry is for N divider on why it is not open. So they find other way for their design and have some confirmations below for SYSREF:

1. Since Ti doesn't open the N divider, then I have to look for other divider, but the RF output channel divider only support even divider ration, it is not a continuous divider, it is still can't be used so I hope the SYSREF could be used
but I'm not sure whether the SYSREF divider is a continuous divider, I'll list it with followed
first , for the SYSREF_DIV_PRE, can I only select div with 1 or bypass it?

2. for the SYSREF_DIV, is it a continuous divider? what's its divide ration range?, from 1 to 2047 or 4 to 4096?

3. finally, for the total SYSREF module, can I select odd divide ration and continuous? for example, can I select divide ration 16, 17, 18, 19, 20, 21...etc?

4. last question is: how about the phase noise floor of SYSREF clock, does it can be same as N divider output clock?
cause i need to use it in PLL design
extremely low noise is required

Please let me know if you have any questions for the customer.

Thanks,

Jonathan

  • Hi Jonathan,

    I'm not sure what is meant by an "open" N-divider... since the channel dividers operate on powers of two, and the VCO range extends from 5.5GHz to 11GHz, normally a continuous frequency range is achieved by changing the VCO frequency and the corresponding N-divider value.

    1. SYSREF_DIV_PRE cannot be bypassed, and must be active to establish a divide value within the nominal interpolator frequency range of 800MHz to 1600MHz.

    2. 4 to 4096

    3. Only even divides are permitted.

    4. The interpolator and the SYSREF delay circuit introduce slightly higher noise overall compared to a standard RF output. Phase noise on the SYSREF output has not been evaluated very closely, because normally as long as the edge jitter is significantly smaller than the delay adjustment step size the overall noise of the SYSREF output is not important to its proper function.

    Regards,

  • Hi Derek,

    Thank you very much for your support in this thread.

    Here's the response of our customer upon sharing your answers:
    To make sure I will not miss anything, I will paste the customer response:

    "Since the channel dividers operate on powers of two, and the VCO range extends from 5.5GHz to 11GHz, normally a continuous frequency range is achieved by changing the VCO frequency and the corresponding N-divider value.' I think there's a misunderstanding about this question.

    As we know, the channel divider only support power of two divide ratio, which means it only support 2, 4, 8, 16, 32, 64...etc divide ratio. Of course it could cover all the output frequency range, but it is just designed for covering the RF frequency range, not for PLL usage. For example, if I want to divide the RF frequency @ 5950MHz to 350MHz, then I need a divide ratio with 17, obviously, the channel divide ratio can't support it. the channel divider only support 350MHz x 16 =5600MHz. cause my application is PLL design, I need a continuous divide ratio to support full frequency cover, just same as N divider, this is why I hope Ti could open the N divider outputs to customer."

    Regarding the "open" N-divider, the customer would like to suggest TI put this outside the IC since it is inside the IC structure.

    Please let me know your comment.

    Regards,

    Jonathan

  • Hi Jonathan,

    I still don't understand the contention by the customer that the channel divide ratio cannot support certain frequencies. True, they cannot support 350MHz from 5950MHz VCO. But they can from 5600MHz VCO with divide-by-16. The whole point of supporting an octave range on the VCO is that it allows complete frequency coverage with power-of-2 dividers. So 5500-11000 is covered by direct VCO output, 2750-5500 is covered by divide-by-2, 1375-2750 is covered by divide-by-4, etc. They can modify the N-divider value to select the appropriate VCO frequency to synthesize any required output frequency.

    Does the customer require a fixed VCO frequency? The use case for this device has been optimized around changing the VCO frequency for synthesizing any frequency down to about 50MHz.

    It sounds like what the customer wants is a fractional output divider. While it would be nice to have an output divider that can synthesize any frequency from an integer PLL, in practice TI makes PLLs with sigma-delta fractional dividers since this is a well-understood architecture, there is digital circuitry composing the fractional component of the divider that must be operating around an order of magnitude higher frequency than the output divide, and consequently the maximum input frequency to the sigma-delta fractional dividers used in our synthesizers is limited to less than 1GHz (internally, the integer portion of the N-divider pre-scales the frequency considerably). The sigma-delta fractional divider approach is great when the output frequency range for the divider is not too high (for example, when the range is equal to the phase detector frequency range) and when the input source is high enough frequency that the digital circuitry can be clocked at high speed relative to the output frequency; but it would not be possible for the sigma-delta fractional divider to take 5500MHz in and give 5495MHz, 2800MHz, or 1.213141GHz out, because all of those frequencies are above the usable maximum output frequency range of the divider. You'll find that the "sigma-delta fractional N-divider + octave tuning range VCO with power-of-2 dividers" approach is standard across the industry, because generating arbitrary fractional divides at high frequency is (as of today) constrained to a range that is better suited for phase detectors than for direct output divides.

    Additionally, we've investigated whether it makes sense to provide the fractional divider as an external component, but when faced with the limitations (<1GHz output frequency, sometimes drastically less, requires an order of magnitude higher frequency clock to drive the digital, added power requirements due to external I/O) most customers would rather just use the PLL synthesizer.

    Regards,

  • Hi, Derek, Jonathan

        Thanks for the long answer! But I'm so sorry I still didn't explain it clearly to you what I mean. I'll  try to describe it much clear for your understanding.

        I think your understanding was just based on single device/single loop design. In single device(single LMX2820 PLL) design case,  It's sure that the channel divider operates at power of 2 conjunction with appropriate VCO frequency range/ N divider ratio could support full output frequency range coverage(synthesis & output),  I have no concern about this. But if we change the thinking, suppose we want to use RF channel divider(it is opened to customer for external usage) instead of using N divider(cause it's output is not opened to customer for external usage), in other word, if I want to use channel divider to replace N divider as loop divider, then I impact the limitation of discontinuous channel divider ratio. For loop divider usage, basically it requires continuous or continuous even/odd divide ratio to meet frequency coverage and  overlay. In this case, reference and divide ratio determines final RF frequency, let's use the same example of above. when I use a 350MHz reference and want final RF frequency 5950MHz, then I must need divide ratio of 17, but the channel divider only support divide ratio 16, which means the final RF frequency I got is 350M x 16 = 5600MHz , furthermore, next divide ratio is 32, which means I can get 11200MHz, the huge gap between 5600MHz and 11200MHz is absent. Hence the RF channel divider can't be used as loop N divider because it is not continuous, this is also why I want Ti to open its N divider output for external usage.

        I don't need TI to open the N divider output for fractional usage, we already have fractional N, what we want is just open the N divider output for customer external usage and only need it to support integer N divide ratio.

       Currently I have give up the attempt of taking channel divider as loop N divider, but I have another question for you which is about 1/f noise, I sent it yesterday on  the post list, pls check it out, thanks a lot!

  • Hi, Derek, Jonathan

        I still have one more question about 1/f noise. the datasheet mentioned it is about -132.5 dBc/Hz @ 1GHz, but not give out its actual noise corresponding to noise floor, so there's confusion here. For example, if I want to calculate 1/f noise of 10KHz offset at 6 GHz, I have 2 methods for that. one is -132.5+20log(6/1) = -117 dBc/Hz; the other way is to get its corresponding noise floor first, suppose to reflect it to 100MHz reference floor, then I get -132.5-20log(1000/100) = -152.5 dBc/Hz, and if I have method to reduce the total loop N to 3(suppose still get to 1 GHz ), then the 1/f noise I can get is -152.5+20log(3) = -142.5 dBc/Hz @ 1 GHz, we can see there's total 10 dBc difference with the datasheet spec, finally I can get it at 6 GHz should be -142.5+20log(6/1) = -127 dBc/Hz. the final results is greatly different, so I wonder if I can calculate the 1/f noise by reflecting it to 100MHz reference? If I can do it, are the calculation and result correct?

      regard

             L

  • Hello L,

    Thanks for the clarification, I now understand what you're getting at regarding opening the N-divider. I think the biggest limitation is that it adds another mux in the feedback path, which impacts the PLL noise performance and the device current; we'd also need to route the N-divider output to some pins, which means either another mux or sacrificing a feature somewhere else. But now that I understand the request and the reasoning behind it, I will keep it in mind for planning future devices.

    The 1/f noise is normalized to 1GHz, but the noise value in the datasheet is given for the 10kHz offset - in other words, we give PN_flicker_10kHz. So to compute the phase noise at 10kHz offset for a 6GHz output carrier, and with the current typical value of -134dBc/Hz, we have:

    PN_flicker = PN_flicker_10kHz - 10log(offset/10kHz) + 20log(Fout/1GHz) = -134dBc/Hz - 0 + 15.56dBc/Hz = -118.44dBc/Hz

    The calculation above matches your result in your first example (slightly different given flicker noise, but otherwise equivalent calculation). Your other method is essentially the same as the first method, but with an additional scaling to 100MHz that changes the result; the extra scaling to 100MHz is not valid.

    Regards,

  • Hi, Derek

           Sorry for responding so late. Thanks for detailed explanation about 1/f noise, but I still have a little confusion about normalized to 1GHz. You know, basically 1 GHz is not a most common used reference frequency, the formula just gives out a typical 6 GHz 1/f noise calculation -134 +20log(6/1) = -118.44dBc/Hz, I think it is much simpler to face different case.  To achieve 6GHz synthesized frequency, suppose using common 100MHz and 500MHz reference frequency, in my understanding of just N, there's 20log(5) = 14dB difference, although include the PFD noise increment of 10log(5) = 7dB, there's total 7dB difference by using 100MHz and 500MHz reference, which means the final 6 GHz phase noise will be 7dBc different. But from the formula, it just only give out a simple calculation which normalize  to 1 GHz, but how to scale it to 100MHz or 500MHz reference(which is much popular in reality)? If I can't scale it to other reference frequency, how to  embody the different phase noise at same 6 GHz by using different reference?  I think the 1/f noise spec normalized to 1 GHz is not appropriate because 1 GHz is not a most common used reference, it's better to specify it at 100 or 200 MHz to represent reality implementation. My design don't use 1 GHz reference, so I have to scale it to my dedicated reference, otherwise I can't get my accurate phase noise calculation, I really need this extra scaling to improve my simulation accuracy and this is very important to meet design goal, expect your kindly help, thanks!

        regards

    L

  • L,

    The 1/f noise is independent of input frequency and PFD frequency. Whether you have a 100MHz, 500MHz, or 10kHz reference, the 1/f noise remains the same. This can be seen with a simple experiment: using PLLatinum Sim (PLLATINUMSIM-SW), load the LMX2820 profile, ensure that there is no multiplier being used in the reference path, and apply any valid combination of input reference and PFD frequency. You will find that the 1/f component of the noise does not change. (The multiplier adds around 1.5dB to the 1/f noise across all frequencies.)

    1/f noise is normalized to 1GHz (and typically given at the 10kHz offset) by convention. We could pick any frequency to set the 1/f noise, but practically we choose the industry convention because it makes it very straightforward to compare device performance both between TI PLLs and between competitor PLLs.

    The 1/f noise only scales with output frequency. You can scale the 1/f noise to any arbitrary output frequency by adding 20log(Fout/1GHz). 

    Since each octave of 1/f noise carries an equal noise energy, it follows from the math that the 1/f noise has a slope of about -3dB/octave or -10dB/decade. Consequently, to compute the 1/f noise for any given offset, in addition to scaling the 1/f noise to the desired frequency, the increase or decrease due to the difference in offset must be included as well, hence the factor of 10log(Offset/10kHz).

    I mentioned it above but I'll focus on it here: TI provides a tool, PLLatinum Sim (PLLATINUMSIM-SW) which can be used to determine the phase noise characteristics for many of our PLLs (including the LMX2820). If you are not already using it, I strongly recommend using PLLatinum Sim to simulate device performance.

    Regards,

  • Hi, Derek

             Now I fully understand the 1/f noise question about LMX2820. As I used to do my simulation by establishing noise model and other parameters, I feel this is rather free to adjust/get what I want, furthermore, Ti's PLLATINUMSIM is not suitable for my special design, it's regret I can't use it. Anyway, I will do some experiments to verify whether the 1/f noise can meet my requirement, thanks for your great helping!

    regards

    L