Hi,
Do we have some products that could help to delay clk signal so that we can match the clk timing to two devices with obvious length difference instead of PCB routing. Do you have some suggestions?
Thanks.
BR
Mason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Mason,
How much of a delay are we talking about? Please also include how many clk signals are needed?
Hello Mason,
The best solution would be to use a zero-delay mode device and matching termination lines. Those factors should be able to be controlled if PCB is not fully designed or matching cables can be implemented.
Hello Mason,
I will be closing this thread as we haven't had a response in a couple weeks.
Please feel free to open another thread if needed.