Part Number: LMK00308
Other Parts Discussed in Thread: LMK00304, , LMK00304EVM
The output skew specification t_SK(O) for the LMK00308 and LMK00304 is only valid for the same buffer type, e.g. LVDS to LVDS. Do you have any skew data for LVDS out to LVPECL out on the same device, that's better than one may calculate from the worst-case difference between t_PD_LVDS and t_PD_LVPECL, i.e. [-340..420] ps, versus as little as 50 ps for t_SK(O)? As long as the temperature is the same (same die) and the load is similar, one might expect somewhat better than this.
Regards,
Torstein Sunde