Part Number: CDCE913-Q1
Hi team,
Could you advise the maximum supply current of CDCE913-Q1 for IDD and IDDOUT parameters below?
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCE913-Q1
Hi team,
Could you advise the maximum supply current of CDCE913-Q1 for IDD and IDDOUT parameters below?
regards,
Hello Shinji,
Please see the Figures 1-3 as mentioned in the Test Parameter, depending on the set Fvco the supply current will change. Is there a set specification you will be using?
Hi Aaron,
Here is my setting. Could you give me the max current with this setting?
Fvco 196.608MHz
Fout 24.576MHz
regards,
Hello Shinji,
This will be an estimate of what your max should be at this setting - again this device has a typical value shown in in Figure 1 of the datasheet - we will estimate with +20% deviation.
The maximum estimate at Vdd = 1.8V, Vddo = 1.8V, Fvco = 196.6 MHz, 3 Outputs on is:
Idd = 23 mA
Iddo = 4 mA