Hi team,
The customer uses LMX2594 to output DAC sampling clock. The input of LMX2594 is 93.75MHZ, VCO = 12GHz, and the output is 6GHz. However, there is spurious at 3GHz. What is the possible reason?
In addition, other debugging conditions:
When VCO = 12GHz, VCO_PHASE_SYNC=1, the spurious frequency is 3GHz; After modifying the VCO frequency of LMX2594, the spurious frequency changes, but it is still VCO/4.
When VCO = 12GHz, VCO_PHASE_SYNC = 0, the 3 GHz spurious signal disappears.