This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Disabling RF outputs

Part Number: LMX2594


Is it possible to disable individual outputs on this part?

If so, what are the risks in doing so?

  • Hi Gregory,

    Individual outputs can be disabled using the OUTx_PD bits. I'm not sure what you mean by "risk" - the output goes high impedance when powered down, and there may be some low-level capacitive feedthrough because of internal high-frequency coupling even while the output is powered down. For better isolation, the powered down outputs may be configured with OUTx_MUX=0x3 (Hi-Z) as long as neither output is configured for channel divider. If you are asking about some other specific risk, please clarify.

    Regards,