This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE6214-Q1: Is it allowed to use multiple outputs?

Part Number: CDCE6214-Q1
Other Parts Discussed in Thread: CDCE6214

Hi,

In the datasheet of CDCE6214, it's stated (tables 11, 12 and 13) that "Multiple output buffers should not be enabled at the same time". Do that mean that i should enable one output, then the other, or that i should never have two outputs enabled at a given time?

In out application, we use OUT1 and LVCMOS output and OUT2 and LVDS output, both generating the same clock. We intend to have both of them enabled.

So, if my understanding is am I allowed to do so with respect to the note above? 

Thank you,