Part Number: CDCEL913
Other Parts Discussed in Thread: CLOCKPRO, CDCE913, CDCE925
I would just like to confirm that the default Slave Address of the CDCEL913 is 1100101b.
I know that address bits A1 and A0 are programmable, and the Configuration Register Map indicates that the default setting for these bits is 01b. But the datasheet also says that if VDDOUT is forced to GND, the two control pins (S1 and S2) temporarily act as serial programming pins (SDA/SCL) and the two slave receiver address bits are reset to A0 = 0 and A1 = 0. Also, when using the Bit Viewer of the ClockPro software, Register 01h displays a value of 00h; so is there an error in the datasheet and the default Slave Address is actually 1100100b, or is the ClockPro software reconfiguring the address bits to a non-default value? If it's the latter and I preprogram my devices using ClockPro (and don't change the SLAVE_ADR value beforehand, does that mean that I will need to use Slave Address 1100100b for future in-system I2C accesses?