This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: LVDS design differences between LMK04806 and LMK04826

Guru 11540 points
Part Number: LMK04828
Other Parts Discussed in Thread: LMK04826, LMK04806

Hello,

For the LMK04826, a 560 ohm resistor should be added when designing the LVDS path with internal receiver termination.

However, in the case of LMK04806, there is no such condition.

Why is there the difference in the LVDS design of the two devices?

Please explain in detail.

Thanks in advance.

JH