Hi
We tried configuring Clkin1 port (J109) as input for providing a reference clock of frequency 10MHz from external reference to the ZCU111 board. For this we have disabled En_Clkin0 and enabled En_CLKin1 in Dual PLL Mode, Int VCO (of LMK04208 in TICS Pro v1.7.2.0) and selected Clkin1 to propagate to PLL1 input through the select MUX. We exported the HEX Register values and configured the clocks through SCGUI. However much to our surprise, we notice Clkin0 continues to propagate with its default frequency of 122.88MHz. This limitation in Dual PLL, Int VCO Mode is preventing us to use PLL1 achieve higher frequencies than the reference clock needed for our design. We are also attaching the Hex Register text files for the below shown two modes.
However in External VCO Mode, We could observe the reference Clock propagate to the ClkOut5 port (J108) through clock distribution network. Hence we could achieve only those frequencies less than or equal to the reference clock (10MHz) for operating the board.
We appreciate if somebody can help us in resolving this issue and help in enabling Clkin1 for referencing the external.