Part Number: LM555
Other Parts Discussed in Thread: REF3433
Hi team,
We have a customer inquiring about the LM555, here are the inquiry from the customer in verbatim:
“I am using the LM555 in astable mode as an LED driver. I will be using nmos transistor as a switch, connected between Vcc and Reset pins of LM555, in order to control the signal into LM555. for this purpose, I will be interfacing the LM555 with a pic microcontroller. the only issue is that I need to change the trigger level of the LM555 to 3.3V, and the datasheets don't provide information on how to do so. Could you please provide me with a solution? Also, please note that the supply is 10.3 ~ 14.8 V battery charged through a solar panel."
Thanks and Regards,
Jenny