Part Number: LMX2571
Dear Support Team;
We use the LMX2571 to do FM modulation. The modulated signal is composed of either a single sinusoidal signal or a composite signal that has a few sinusoidal components.
We demodulate the signal using universal demodulator after analog FM modulation using SPI-FAST. We are sure that the demodulator works perfectly (We have tried various FM demodulation setups including sofware defined radio – GNU Radio to be specific.). But when we measure the phase of the demodulated signal, we observe that the PHASE of the demodulated signal is not constant and changes over time. So although we expect constant and stable phase on the demodulated signal, we keep loosing the phase information.
Our test setup information is as follows:
Our test setup consists of STM32G431KB for the SPI interface and LMX2571EVM for FM modulation. First, the modulated signal is oversampled(80kHz) and then sampling information is written to flash of the STM32G431KB. Then the samples of the composite signal is written to R33 register of the LMX2571 for the FM modulation. The maximum deviation is about +/-20 kHz and the cycle rate is between 100Hz to 15kHz. (DEN=5394304, CH1=4, Ch2=8, fPd=120MHz, prescaler=4, Loop BW=204.8kHz)
Is this to be expected for LMX2571? Can we obtain FM modulation with no or negligible phase corruption?
What might be the possible cause of the problem?