Part Number: CDCEL913
Other Parts Discussed in Thread: CLOCKPRO, , CODELOADER, USB2ANY
Dear,
I want to use ClockPro to generate 24MHz clock setting for CDCEL913. However, after I sending Byte 27, CDCEL913 returns to default value, bypass the input crystal clock(25MHz crystal) to output.
I have tried many times, all failed.
Could you help to check is there something wrong about this setting ?
Here is the setting saved from ClockPro.
Thank you.
| Bit => | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |||
| Byte0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 00000001 | 1 | |
| Byte1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte2 | 1 | 0 | 1 | 1 | 0 | 1 | 0 | 0 | 10110100 | B4 | |
| Byte3 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 00001001 | 9 | |
| Byte4 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 00000010 | 2 | |
| Byte5 | 0 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 01100000 | 60 | |
| Byte6 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 01000000 | 40 | |
| Byte7 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte8 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte9 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte10 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte11 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte12 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte13 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte14 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte15 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte16 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte17 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte18 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte19 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte20 | 0 | 1 | 1 | 0 | 1 | 1 | 0 | 1 | 01101101 | 6D | |
| Byte21 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 00000010 | 2 | |
| Byte22 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte23 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 00000000 | 0 | |
| Byte24 | 1 | 1 | 1 | 1 | 0 | 0 | 1 | 1 | 11110011 | F3 | |
| Byte25 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 00000011 | 3 | |
| Byte26 | 1 | 1 | 1 | 1 | 0 | 0 | 1 | 0 | 11110010 | F2 | |
| Byte27 | 0 | 0 | 1 | 0 | 0 | 1 | 1 | 1 | 00100111 | 27 | |
| Byte28 | 1 | 1 | 1 | 1 | 0 | 0 | 1 | 1 | 11110011 | F3 | |
| Byte29 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 00000011 | 3 | |
| Byte30 | 1 | 1 | 1 | 1 | 0 | 0 | 1 | 0 | 11110010 | F2 | |
| Byte31 | 0 | 0 | 1 | 0 | 0 | 1 | 0 | 0 | 00100100 | 24 |
Brs,
Leon