Part Number: LMK1C1104
I would like to use the LMK1C1104 with either an LVCMOS or sinewave input at 40MHz. With a 3.3V supply, what is the MAXIMUM input slew rate, i.e., will it work with a sinewave? The data sheet only specifies minimum slew rate.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK1C1104
I would like to use the LMK1C1104 with either an LVCMOS or sinewave input at 40MHz. With a 3.3V supply, what is the MAXIMUM input slew rate, i.e., will it work with a sinewave? The data sheet only specifies minimum slew rate.
Hi Barry,
The slew rate specification is for 20% to 80%. So a sine wave actually does get moving well enough here that at 40 MHz you can meet the slew rate specification. For example:
40 MHz @ 3.3 V from 20% to 80% is 0.387 V/ns, risetime = 5.1 ns
40 MHz @ 2.5 V from 20% to 80% is 0.293 V/ns, risetime = 5.1 ns
40 MHz @ 1.8 V from 20% to 80% is 0.211 V/ns. risetime = 5.1 ns
As for maximum rise time, since we specify slew rate, the maximum allowable rise time becomes a function of amplitude. The larger amplitudes have longer allowed rise times. In my example above, the slew rate increases because I hold the frequency (which is associated with rise time) constant while increasing amplitude.
So for a 3.3 V signal, a 10.5 MHz sinewave would have just over a 0.1 V/ns slew rate with a rise time of 19.5 ns.
For a 1.8 V signal, a 19 MHz sinewave would have about 0.1 V/ns slew rate with a rise time of 10.8 ns.
Of course supply isn't always exactly 3.3 V or 1.8 V.
Hope this helps.
73,
Timothy
Thanks, Timothy.
I wasn't thinking quite clearly (apparently) when I posted this. This makes perfect sense.
TU,
Barry