Hi, support team.
I can see programming cycles, Min 10 cycles, Max 10,000 cycles, in the datasheet.
Then I have questions.
1. What does "Min 10 cycles" mean ? Isn't it too little?
2. What does the "cycles" mean?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, support team.
I can see programming cycles, Min 10 cycles, Max 10,000 cycles, in the datasheet.
Then I have questions.
1. What does "Min 10 cycles" mean ? Isn't it too little?
2. What does the "cycles" mean?
Best Regards,
Hi,
Let me ask you additional question about cycles.
If we write data to an address (ex. 0x00), is it one cycle?
Then for whole address (0x00-0x3F), is it 64 cycles?
If so, I think "Min 10 cycles" is not appropriate.
Best Regards,
Hello,
If we write data to an address (ex. 0x00), is it one cycle?
It is one cycle for address 0x00.
Then for whole address (0x00-0x3F), is it 64 cycles?
No, it is one cycle for each address from address 0x00 to 0x3f.
If so, I think "Min 10 cycles" is not appropriate.
So you can achieve ten full programming programmings.
73,
Timothy