Part Number: CDCE62005
Other Parts Discussed in Thread: TMS320C6678, LMK03318, CDCE6214
Hello,
Since we are starting a new design with the TMS320C6678, I understand that the CDCE62005 is a good choice to provide the LVDS clocking for the DSP: 100MHz for the core, 50MHz for the DDR, and 250MHz for the SGMII. Please let me know if that is my best choice first of all. Assuming that is reasonable, what I'm trying to figure out is the programming. Of course I plan to connect the SPI interface of the DSP to the CDCE62005. My second question is after I have worked out how to program the registers in the CDCE62005, how would the factory program the CDCE62005 before they solder it onto the board? My third question is that if we have a problem with our prototype boards such that the DSP is not running well enough to reprogram the CDCE62005, is there a way to re-program the CDCE62005 in-system?, maybe by connecting a header to the SPI pins and using some kind of programming cable/adapter from a PC?