Part Number: LMX2571
Questions about LMX2571
On page 44 of the data sheet, you will find information on setting the Synthesizer Duplex Mode Tx902MHz, Rx 928MHz, and FSK modulation modes.
Table 41. The DEN setting value is 0. Is it better to use 0 for the DEN setting value when using it for FSK modulation?
Also, could you please give me the configuration file in TICS PRO for FSK modulation measurement described on page 44?
The reason is to evaluate with the evaluation board you purchased.
LMX2571に関する質問です.
データシートの44ページに、シンセサイザーデュプレックスモードTx902MHz、Rx 928MHz、およびFSK変調モードの設定に関する情報があります。
表41.DEN設定値は0です。FSK変調に使用する場合、DEN設定値に0を使用する方が良いですか?
また、44ページに記載されているFSK変調測定用のTICSPROの設定ファイルを教えてください。
購入した評価ボードで特性確認をするためです。