Hi,
I'm currently working on a POC of a spatial radar for asteroids and we will start characterization on a first prototype for end of next june.
The frequency range is [300; 2500]MHz and I've had a look on some PLL components for the global architecture.
I've identified the LMX2615-SP that could be a good candidate but for which I have a couple of questions :
1-) What is the output power at 300MHz ? 800MHz ? 2400MHz ?
2-) Is a common output matching network could be used for that broad frequency range ?
3-) The datasheet gives only closed-loop phase noise; do you have also the open-loop phase noise @10kHz offset ? frequencies of interest are 800MHz and 2400MHz.
4-) Do you confirm that it is space qualified ?
Best Regards,
Hervé Guidetti