Hi,
In a new design we are going to use the LMX2820 as PLL. We must use as reference an external 50 mhz sinewave signal, which power level goes from -10 to 15 dBm.
To avoid burning the PLL, we will use an HBT amplifier with low phase noise working in saturation, but we have many doubts:
-Is the approach correct?
-If the answer is yes, shall we filter the signal?
-If the approach is non-correct, instead of using an amplifier, What can we use? Maybe a clock cleaner?
-What is the minimum input level that the LMX2820 can support without increase the phase noise?
Thanks and best regards,
Aizkibel