This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: Alternative clock for the ADS42LB69 ADC

Part Number: LMK04828
Other Parts Discussed in Thread: ADS42LB69, , LMX2594, LMX2572, LMK03328, LMK03318

I have an ADS42LB69 ADC that is being driven right now by a SiLabs Si5326.  I don't think the Si5326 has good enough jitter specs to have this device meet TI's datasheets specs for this ADC.  TI has the LMK04828 but this is a fairly big part with too many clock outputs.  I only need enough clock lines to drive two ADC's.  My needs are way less than 14.  Is there an in between clock device that would work for this 16 bit ADC?