Part Number: LMX2820EVM
Other Parts Discussed in Thread: LMX2820, LMX2492
Good afternoon
We're looking at implementing the LMX2820 in a ramp generator system and I'd like to program the LMX2820 to a fixed centre frequency and then ramp the reference input frequency so that the PLL follows the reference input without reprogramming/calibrating the PLL/VCO.
Various measurements at different frequencies indicates the PLL can 'hold' lock to the reference input frequency from between a few MHz to 50MHz depending on settings.
Can someone tell me what the parameters are that have an impact on the hold range of the PLL over the reference input frequency please?
The implementation is to set a particular reference frequency generated by a DDS and then to lock the LMX2820 to this reference input and a particular RF output. The DDS reference frequency will then be tuned over a 50MHz range with the ramp translated onto the VCO. I am using PFDin with a feedback mixer for low phase noise.
I've read various control theory and PLL tech notes but can't find anything relating the PLL transfer function (including loop filter) to the reference input bandwidth. I did initially think it may be related to the loop filter bandwidth but increasing and decreasing the LBW didn't make much difference to the hold range.
Many thanks and I look forward to hearing from you
Best regards
Jon