This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCS502: Input signal requirements

Part Number: CDCS502

Hi expert,

My customer is using CDCS502 for adding SSCG function.

However they have an issue about amplitude for input signal.

Their waveform meet VI threshold, but it didn't meet VIL/VIH.

input signal

Vdd = 3.3V

Max = 1.9V < Vdd x 0.7 = 2.31V

Min = 1.14V > Vdd x 0.3 = 0.99V

Could you please give me your advice? Will they need meet VIL/VIH spec?(or is it no problem because the waveform is oscillate around Vi threshold?)

Thanks

Muk