This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DS080: Comparison of ADC12DS080 and ADC3222

Guru 11355 points
Part Number: ADC12DS080
Other Parts Discussed in Thread: ADC3222,

Hi,

I have a question about ADC12DS080 and ADC3222.

1. Each has the following description.

- ADC12DS080: Full Power Bandwidth (-3 dB Corner) 1000MHz

- ADC3222: Analog input bandwidth (3dB) 540MHz

The notation is different between "Full Power" and "Analog input", but do they have the same meaning?

 

2. Is there a frequency characteristic diagram for each device?

I want to know the frequency if it can be used without attenuation around 0.5dB down.

 

3. Min of sampling frequency was not described.

I want to know the lower limit of each operation.

Thanks,

Koki