Can you provide detail example schematic for ADS62P42 and TRF371125 connection.
system request:
1. I/Q Frequency response: 0~30MHz
2. Low DC offset
3. Low noise floor
4. I/Q Balance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
A good example schematic will be the attached TSW6011 EVM schematic. The connection between the TRF371125 and the ADS62P42 (or ADS5282 in the TSW6011 EVM) is a direct DC couple connection. You will need to route the VCM output of the ADC to VCM input (pin 24) of the TRF3711.
-KH