Hi Team,
We have received this inquiry from our customer.
Regarding the ADS1278-EP device: two devices that work in parallel.
Our system works with two ADS1278-EP in "high speed" protocol and SPI protocol in parallel.
CLK = 13.5MHz;
CLKDIV =1;
SCLK = 12MHZ;
The goal is to sample simultaneously by the two ADS's when the accuracy of the sampling time difference between the two devices should be better than 8 microsecond. Is there an application that meets this requirement?
Regards,
Danilo