PPG CHIP |
P/N |
ADC Resolution |
SNR |
FIFO |
DC Ambient Rejection |
DC Ambient Range |
Work Power Consumption |
Shutdown Power Consumption |
Package Size |
AFE CHIP |
TI 44i30 |
20bit |
108db? |
128 word |
100db/ 10Hz? |
255µA |
23.5uA @xxsps? |
uA? |
DSBGA-30 2.6*2.1mm |
Hi team,
- is that the maximum SNR is 108dB when PFR=1600Hz, DR=50Hz, signal current=16uA? Is that signal current more than 16uA, the SNR will be higher?
- How much is the SNR nyquist if there has?
- Is that power consumption is RX_SUP current+ IO_SUP current+ TX_SUP current= 21+1+1.5=23.5uA?
- About hardware shutdown's power consumption, it shows RX_SUP current+ IO_SUP current+ TX_SUP current< 1uA, but is there any more detail data, such as <2uA or <1uA to make sure this device is more competitive.
- About DC Ambient Rejection, is there the data of 120Hz?