Hi Team,
I am using ADC12DJ3200 in my design. I want to confirm about the output lane rate for the JMODE 12.
Case1: As mentioned in the datasheet the lane rate would be Devclk multiplied by the factor R. and R is derived as 1 for the JMODE 12. so, the lane rate will be 3.2Gsps*1=3.2Gbps.
Case 2: But if I calculate with below formula
lane rate= [M*N'*(10/8)*Fdecimated]/L
lane rate = [8*12*(10/8)*800]/8 =12Gbps ; all the parameters are taken for JMODE 12, Fdecimated=3200/4=800Msps
So, both the cases the lane rate is different. which case is to be considered for the lane rate calculation.
Please do the needful.
Thanks & Regards
Saisri Bhairi