This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL0401A-10: Equation for Output Voltage Configuration

Part Number: TPL0401A-10

On Page 13 of TIDU533, equation 24 shown below shows how to calculate R11. When I try to use the given example I get nothing shown in the photo.

R10 = 2490 ohms

Vmax = 15 V

Vmin = 5 V

Rpotmax = 7500 ohms

Rpotmin = 0 ohms

Vref = 0.8 V(given on page 12)

Solving for R11, i get -8.874 ohms, and obviously I'll also get the wrong answer for R7 using that. Did I miss something simple here and just bad at math or is the equation wrong?