Other Parts Discussed in Thread: ADS1115, TLA2024, ADS1015
Hi Team,
I am experiencing similar problems outlined in this E2E post. The ADS1115EVM-PDK is not being recognized by the GUI, I was able to follow the steps outlined in the post, however, I get to a point where the EVM powers down and I no longer see the "Generic Bulk Device" in Device Manager. I've updated the driver for this device using the usb_dev_bulk_comp multiple times. If you can lend some help debugging this issue, it would be greatly appreciated. Thanks!
1.) Get connection failure when starting GUI
2.) I am able to switch com ports, I see the warning about EVM unrecognized, close warning, and then see the below screen. I am also able to see the device in Device Manager at this point with the EVM powered on
3.) I go to File -> program device. EVM powers off (no lights on EVM) and is no longer shown in Device Manager
4.) I am able to go to file - > program device again, select ADS1115, however, it doesn't matter since device is unconnected. Warning for unsuccessful flash shown. GUI automatically refreshes after a few seconds
Best Regards,
Vijay