This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello, jim
My custom board can work normal when setting as follows
Fdata = 300M
LMF =442
interpolation = 4
Fdac = 1200M
SerDes Linerate = 6000M
but when I double the interpolation to 8, Fdac to 2400M, it can't sync. I have modified three registers
reg 4x 8x
0x25 0x4000 0x6000
0x3b 0x800 0x1800
0x00 0x218 0x418
the clk is generated by lmk04828, vco is locked to 2400M, when divider = 2, it output 1200M to dac, when divider=1, it output 2400M to dac。then how to check hardware?
Xiao,
I got this mode working with the TI EVM's. The register settings are attached.
Regards,
Jim