Other Parts Discussed in Thread: LMK04828
Hello Every One,
I am planning to use ADS54J66 ADC for the input Frequency of 650MHz to 700MHz range.
I have not seen SNR and SFDR performance in Datasheet for that frequency.
I referred the performance attached in the below Link.
But these plots are taken with -4dBFS Fundamental Power.
It will be very helpful if you are providing the following results.
1)The tested plots with -1dBFs Fundamental power in few frequency spots from (650MHz to 700MHz)
2) The Phase Noise data of the Sampling Clock provided to ADC.
3) Input Power at which -1dBFs is reached as per the ADC front end design in Evaluation Board.
Thanks in advance,
Vigneshwar Raj