This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1675REF: Fast ADC (>1MSPS) with low error (<0.5mV)

Part Number: ADS1675REF

I am looking for fast ADC chip that can produce 1M sample per second with less than 0.5mV error. TI's ADS1299 is a good ADC chip widely used in EEG HW. Its error can be less than 0.1mV with 250 sample rate. However its max sample rate is only 16k.

ADS1675 seems a good choice. I wonder if there is any breakout board for it. Its evaluation board is rather expensive $499.