Other Parts Discussed in Thread: ADS131E08
Hello,
I'm using the ADS131E08S ADC in a project I'm working on. The Vref voltage is 4V because the ADC is powered by 5v. However, in my own application, I need to cancel the internal Vref regulator, and instead of the internal regulator, I need to use a 2.5V external reference regulator. Is it possible to cancel the internal reference regulator? I can run the ADC by using an external 2.5V regulator in the products with the same manufacturer code, namely "ADS131E08S", that I bought in previous years. However, I cannot provide this for products that I have recently supplied. Can you help with this issue?