This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102: Does the space qualified part use the same die as the commercial part?

Part Number: ADC128S102
Other Parts Discussed in Thread: , ADC128S052-Q1

Is it just a binning process based on temperature? Or are the dies actually different?

  • Hello Jack,

    We do not provide die/design information on the public forum.  We can confirm that the commercial ADC128S102 and automotive ADC128S052-Q1 devices will not pass the same SEL and TID ratings that the ADC128S102QML-SP due to differences between the -SP product from the other two.