Part Number: ADS1299
Other Parts Discussed in Thread: ADS1263, TLV2771, TLV6742, OPA337, OPA2625
Hello!
I am working on an application using a piezoelectric sensor (disk). I have tried to use ADS1299 and ADS1263 to acquire the signal from the sensor and it has worked quite well. But the piezoelectric sensor is a high impedance sensor and has some problems in reading low frequency signals, which is my main goal (0.1 to 100 Hz). So, I would like to know if it is possible to use ADS1299 and ADS1263 for this task and which one is better. Is there a better part on the market for this application (amplifier + ADC)? Is there a specific analog front-end designed for this application (piezoelectric sensors)?
Best Regards,
Mateus