I have a question about the contents of pages 36-38 of the AFE4490 specification.
Since the clock is 4MHz and the total count of EXAMPLE in Table 2 is 8000,
1 / 4MHzX8000 = 2ms. I understand that the PRP in Fig64 of the timing chart is 2ms.
Is it possible to shorten this measurement cycle of 2ms to 1ms?
If the 8MHz clock is changed to the 16MHz clock in Fig59 on page 33, IC will become inoperable.
Is it possible to set the register to acquire only the data of either LED1 (IR) or LED2 (RED)?
I understand from the specifications that such a setting is not possible.
The purpose is to change the measurement cycle from 2ms to 1ms.