Part Number: TLV2548-EP
Other Parts Discussed in Thread: TLE2022, TLV2548
I am getting some unintended adjacent channel to channel coupling between an input channel of maximum input voltage (say 4.095V), and the adjacent channel of 0V.
The inputs to the ADC is driven by a TLE2022 configured as a follower, so the source impedance is relatively low.
While the datasheet specifies the Input MUX On Resistance at 500 ohms, and the input capacitance at 50pF (assumed to be sample and hold cap value), what is not specified is the resistance of the sample and hold switch.
Could someone provide a more detailed description of the input structure of this device so setting time can be analyzed ? I have attached a small drawing showing my vision of this structure.
Thanks.