Hi all,
I am designing a ADC circuit using ADS7854 and utilizing its fully differential input configurations.
From the datasheet, there is a 16 bits Configuration Register (CFR) (page 34).
I am required to configured the CFR to enable my desired input configurations.
My question is that, what would happen if I write a 1 to bit 8 | 7 | 4 | 3 | 2 | 1 | 0. Because those bits field are 0 and also written in the datasheet that these bits must be set to 0 (default).
Thank you.