Hello,
My customer has a few questions about the ADC12DJ3200QML-SP.
They want to use the ADC12DJ3200QML-SP with the following conditions.
- Dual-channel mode with DDCA, 16 decimation 2 lanes or 1 lane
- Input Signal : approx. 3.6GHz, using channel A only / channel B left unconnected (not used)
- Sampling CLK : approx. 2Gsps
Q1. Is it possible to use the ADC12DJ3200QML-SP with the above concept ?
Q2. If only A channel is used in dual-channel mode to use DDCA, should I leave the unused B-channel unconnected? or should do something?
Q3. For permanent power saving on unused B channel, how to use power down mode only for B channel without damage of output serializers while long time Power down.
Thank you.
JH