Other Parts Discussed in Thread: THS4131,
Hello,
I considering AD conversion circuit that circuit is used ADS8422 and THS4131.
I considering this circuit based on figure 29 of ADS8422 data sheet.
THS4131 negative output is connected +IN of ADS8422 on figure 29.
And THS4131 positive output is connected -IN of ADS8422 on figure 29.
I would like to confirm polarity of AD conversion data at below condition.
Conditions:
- Positive input (390ohm side) of THS4131 is positive voltage.
- Negative input (390ohm side) of THS4131 is 0V.
Regards,
MESH