The Device has only one supply pin. What is the SDO and EOC/nINT voltage level? The that sheet shows the VOH (min). But it does not tell me if the pin has no load. In normal usage, the input port of its master device is in high impedance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Device has only one supply pin. What is the SDO and EOC/nINT voltage level? The that sheet shows the VOH (min). But it does not tell me if the pin has no load. In normal usage, the input port of its master device is in high impedance.
Hi Xiang,
Please refer to the test conditions noted in the TLV2548-EP datasheet for Voh. If there is 'no load' the outputs will not exceed Vcc.