Part Number: DAC3164
Other Parts Discussed in Thread: OPA625, , TINA-TI
I'm looking at using a current source DAC (such as the DAC3164) feeding a voltage-feedback buffer amplifier (such as the OPA625).
The application calls for a unipolar output (0.1 to 1.6V out). It's desired to power the buffer amp from 3.3V.
Looking at SLYT360, it is straightforward to set up the amplifier for the proper input impedances, gain etc.
What is not covered (and what I need help with) is deriving the circuit changes needed to provide offset such that I can use the full resolution of the DAC over the output voltage range. I think this means that an offset needs to be fed to the buffer amp stage to bring the output to roughly 0.8V when the DAC output is at midrange.