Part Number: ADS1282
Other Parts Discussed in Thread: OPA4277, ADS1118, ADS131M02, ADS1262, ADS1256
Hi..
One of my customer is working on high resolution temperature controller & they have considered ADS1282 for their project.
They have used OPA4277 as front end & made differential amplifier using 2 opamps in buffer mode. No gain from OPAMP, only low pass filter is implemented with OPAMPs. Design is working fine accept one issue.
After power on when they are capturing the data (clock - 1 MHz), after 30 samples they see the drop in count & hence they have to discard the 30 samples initially. After that it remains on the same level. This variation is about 80 to 100 counts. We would like to know what could be the issue or is it the known behavior.
Pls. find below snapshot.