Hello guys,
One of my customers is evaluating AMC3306M25 on their own board. their board has one AMC3306 and they assembled 30 sheets of the board.
They observed DCDC_OUT terminal voltage of AMC3306M25 high side on each board. In the result, they found DCDC_OUT voltage on 3 or 4 sheet were about 1.86V not typical voltage(3.5V). Also HLDO_OUT voltage was almost zero when DCDC_OUT is 1.86V.
One of 2 channel opamp IC, one of 1 channel opamp IC, two of 0.1uF bypass capacitor and total 40kohm voltage divider are connected to the HLDO_OUT.
This DCDC_OUT voltage drop phenomenon is happened sometimes. And the phenomenon is disappeared when the power of VDD is turned off and on again.
First question are the below.
Q1. Do you know a phenomenon like this and do you know what the cause is? Is there any countermeasure?
I have another question.
Q2. The device datasheet shows device startup timing at Figure 6-2 on page 10.
I think CLKIN signal should be started to input after VDD powered up.
Is there any timing limitation between VDD power up timing and CLKIN signal start timing?
For example, is it OK to start CLKIN signal input after 100ms elapsed from VDD powered up?
Your reply would be much appreciated.
Best regards,
Kazuya.