Hi
I use ADS1602 to translate voltage to numerical value.
I use external vref, Vrefp=4V, Vrefn=1V, Vmid=2.5V, so I know my input can be differential Vin=3V.
But I read data, when Vin=0.5V, the numerical value=230xx(2V), Vin=0.3V, the numerical value=138xx(1.2V).
There's always a 4-times than it should be. Is there a times-adjustment at ADS1602?
If yes, how to adjust times?
Thanks.