Other Parts Discussed in Thread: ADC12DJ3200EVM, , LMK04828
Hello,
I am using the DAC39J84EVM in conjunction with the ADC12DJ3200EVM to operate as data converters respectively in transmitter and receiver of a bespoke optical communication system.
Given that the clock reference of the ADC EVM is 100MHz, provided by the CVHD-950-100.000 oscillator, I would like to have the same oscillator as a frequency reference in the DAC.
Looking at the user guide for the DAC it looks that I have potentially two options (maybe more):
1) Use the external reference clock and send in input the signal generated by an external board which should contain the CVHD-950-100.000. This could be done through J17 of DAC39J84EVM.
2) Physically modify the DAC39J84EVM and place CVHD-950-100.000 instead of Y1, which is currently CVHD-950-122.880. The reason why I would go for this option is because it is cheaper and quicker to achieve, given that I don't have to design a new board to hold the oscillator.
Given that my plan is to use the DAC39J84EVM with the TSW14J56 (or 57) with the HSDC GUI and the DAC GUI, is any of the above solutions more convenient? For example, would a change of Y1 create troubles in the GUIs, given that the reference won't be 122.88MHz?
Kind regards,
Francesco