Other Parts Discussed in Thread: AMC1035
Dear support forum,
in our project, we have two different AMC1210.
One is using 20MHz for both the modulator and system clock (AMC1210_20_20), the other one is using 20MHz for the modulator and 25MHz for the system clock (AMC1210_20_25). All Clocks are externally connected to the AMC1210.
With the AMC1210_20_25, we don't seem to have any issues. On the AMC1210_20_20 however, in dependence on the voltage level of the measured quantity, the modulator failure occurs from time to time.
Because the only difference in the setups is the system clock frequency, we ask ourself, whether it shall be avoided to use the same frequency for both, the system and modulator clock.
Kind regards
Sebastian Schöler